Home ยป Project Browse

Search for projects in all categories

 
 Include Trove Categories In Search

Full name
alternative text
Account name (lowercase)
alternative text
Description
alternative text
Rating
alternative text
WilLink8 Releasewilink8_filesShare and hold Wilink8 release files(Project not rated)
WiLink Connectivity Drivers for OMAPwilink_driversProject develops Open source drivers for TI's WiLink (including WL1271) Solution for OMAP. (Project not rated)
Titan - Texas Instrument Test AutomatioNtitanTitan is a Test Automation Tool powered by Java and developed to run Linux Kernel test cases.(Project not rated)
TIMotorLIBtimotorlibThe aim of this project is to introduce TIMotorLIB. TIMotorLIB is an open source library in the terms of LGPL license. The proposal of this library is to achieve fast development of digital control systems, mostly focused on the control of power converters, using Texas Instruments TMS320F28XXX Digital Signal Controllers (DSC) based boards. The development of this code has been done using the eZdsp F28335 board from Spectrum Digital. The library is programmed using C as the main language, although additional contents can be developed using TMS320C28x assembler (F28XXX CPU).(Project not rated)
TI81xx A8 Host Utilitiesti81xx_a8utilsTI81xx A8 Host Utilities are a set of useful utilities which can be used by users for debug and profiling from A8 Host side on TI81xx platform. Currently its implemented and tested for TI816x but is portable to TI814x. Includes utilities for - Remote Processor Printf - DDR/L3 System Priority Set/Get - Register / Memory Rd/Wr - Ethernet + SATA use-case profiling - EDMA user space exported APIs - Syslink load and debug utilities(Project not rated)
TI OMAP4 Blaze TabletblazetabletThe project develops and ports Android for TI OMAP4 Blaze Tablet Platform.(Project not rated)
TI Embedded Speech RecognizertiesrThe TI Embedded Speech Recognizer (TIesr) is a set of fixed-point APIs implementing speech recognition. It balances resource usage, robustness to environment, and performance, and has an easy-to-use interface. This makes TIesr an excellent recognizer for developing a wide variety of voice-enabled embedded applications.(Project not rated)
Symbian Foundation on OMAPZoomomapsymbianTI ZoomII baseport for Symbian^3(Project not rated)
Support ProjectsupportSite Support Project(Project not rated)
SteelheadsteelheadThis is a project to support Google Nexus Q running AOSP Android on top of TI 3.0 kernel(Project not rated)
Sitara Flash ToolsitaraflashtoolSitara ARM Microprocessors Flash Tool for AM335x and following devices.(Project not rated)
SGX GraphicsgleslayerThis project provides necessary additional packages for Graphics software from TI. This currently includes XgxPerf - a development and performance benchmarking toolkit for Qt framework and SGXPERF for SGX530. A GLES renderer for the OGRE3D Gaming Engine is already part of OGRE mainline. (Project not rated)
qt-demosqt-emb-demosqt based demos for arm embedded processor(Project not rated)
PRU Softwarepru_swSoftware for TI's Programmable Real time Unit (PRU), including Linux driver & samples(Project not rated)
Pin Setup for AM18xxpinsetup_am18xxPin setup utility for AM18xx devices(Project not rated)
Pin Mux Utility for Sitara ARM MPUpinmuxutilitySoftware tool for evaluation of pin muxing options for Sitara ARM MPU and related devices.(Project not rated)
panda-binariespanda_binariespandabord binary files(Project not rated)
OpenMax for OmapopenmaxThe project contains TI's OMX components written on top of accelerated DSP codecs. (Project not rated)
OpenLinkopenlinkTI's wireless solution for community(Project not rated)
omapreg_debugomapreg_debugThis module provides read/write access to the complete system space using the DebugFS interface. This is similar to devmem2 userspace tool. But certain registers in OMAP architecture can be accessed only in supervisor mode. This tool provides this using the DebugFS interface. For example, the pinmux registers in DM816x and DM814x platform cannot be written from userspace. This module will be helpfull in this case. This is just a debug module which could build separately and used. The same module should also work on all 32-bit CPU architectures (not only ARM/OMAP).(Project not rated)
OMAPpediaomappediaFiles and Docs for Omappedia.org(Project not rated)
OMAP ZoomomapzoomSupport collaboration around the OmapZoom MDP.(Project not rated)
OMAP SYSLINK / BIOS IPCsl_bios_ipcBIOS IPC in Syslink includes the inter-process communication components running on the subsystems, i.e. DSP or Cortex-M3.(Project not rated)
OMAP Support ToolsomaptoolsOMAP Support Tools(Project not rated)
OMAP SGX Graphics Drivers for AndroidomapgraphicsThis project maintains the Graphics SDK for the OMAP3/4 platforms running the Android OS(Project not rated)
OMAP Releasesomap_binrelOMAP Binary releases(Project not rated)
OMAP Linux KernelomapkernelKernel support for OMAP processors(Project not rated)
OMAP DSP BridgeomapbridgeOMAP ARM/DSP Bridge Driver(Project not rated)
OMAP Domain ListsomapdomainThe aim of this project is to provide public domain support lists for various OMAP domains & subsystems(Project not rated)
OMAP Boot LoaderbootloaderBoot loader for OMAP processors(Project not rated)
MSP430 MMC Codemsp430_mmc_codeTI low-cost Multicore C64x and C66x DSP EVMs are compatible with the AMC form factor and can be plugged into an AMC chassis. The on-board MSP430 acts as the MMC and interfaces with the system's MCH. This is the code and project files that runs on the MSP430.  Comments...
Mini FilesystemminifsSmall embedded filesystem for quick development(Project not rated)
Medical Imaging Demo Application Startermed_ultrasoundTexas Instruments' Medical Imaging Demo Application Starter (MIDAS) illustrates the integration of key medical imaging algorithm modules on Texas Instruments (TI) DSPs and System-on-Chips. (Project not rated)
Media Controller Utilsm_c_utilsContains utility software to load the Media Controller firmware from Cortex A8.(Project not rated)
matrix-gui-v2 appsmatrixguiv2appsHosting for smaller matrix applications icons, description pages, and desktop entries.(Project not rated)
Matrix TUI Launcher Applicationmatrix_tuiThe Matrix TUI (Text User Interface) is the complement UI to the Matrix GUI project. Using ncurses, it is designed to provide a text user interface on the console that creates a hierarchy and ease of use for the example applications and demos that exists in the TI ARM Cortex-A8 SDKs. It's functionality and available applications & demos mirrors that of Matrix GUI. The TUI uses a .xml file which is parsed by libxml to create the main menu and supported submenus. Like the Matrix GUI, additional applications and demos may be added by simply modifying the existing .xml file. (Project not rated)
Matrix GUI Launcher Applicationmatrix_guiThe Matrix GUI is a launcher application being developed for the TI ARM based SoCs. The GUI is a simple .html page that is developed using Qt/webkit. The 3x4 or 2x4 matrix of icons calls existing example applications and demos and makes them accessible to the user. Additional applications or demos may be easily added by simply modifying the existing .html file. The GUI is touchscreen, mouse and keyboard enabled and enhancements can be made by the users using the Qt SDK. Matrix is intended to address the ease of use and quick OOB experience. It is also meant to serve as the baseline for our SDKs that will allow users to extend existing applications or create their own. (Project not rated)
Matrix Application Launcher v2matrix-gui-v2The Matrix GUI is a launcher application being developed for the TI ARM based SoCs. The 3x4 or 2x4 matrix of icons calls existing example applications and demos and makes them accessible to the user. Additional applications or demos may be easily added by simply adding a new desktop file into the target file system and refreshing Matrix. Matrix works either by touchscreen or mouse and keyboard on the target or remotely through an external browser. Matrix is intended to address the ease of use and quick OOB experience. It is also meant to serve as the baseline for our SDKs that will allow users to extend existing applications or create their own.(Project not rated)
Low Level Driver Exampleslld_examplesThis project contains examples for programming the EDMA3 with the LLD (low-level driver) library.(Project not rated)
IPCipcIPC - discussion for projects hosted at http://git.ti.com/ipc/ipcdev(Project not rated)
Integra ApplicationsintegrademosThe purpose of this project is to develop demos and example applications for the Integra EZSDK on C6A8 devices.(Project not rated)
GStreamer on TI DaVinci and OMAPgstreamer_tiThis project develops a GStreamer plugin for TI DaVinci and OMAP3 platforms to utilize the DSP and other hardware resources for accelerating streaming audio and video processing and image manipulation. (Project not rated)
FlashflashThis project is for the development of an application which provides users the capability to prepare a target board to execute a bootloader residing in peripheral memory devices. The primary function of the application is to store a bootable image to the flash memory of the target device (though other functions exist). It will support the current generation of ARM MPU devices (OMAP 35xx, 37xx, AM 35xx, AM/DM 37xx) as well as roadmap devices.(Project not rated)
FCfcdevFramework Components developers - discussion for projects hosted at http://git.ti.com/mfp/fcdev(Project not rated)
example project for demonstrationexample_projectThis project is an example workspace to demonstrate how to use the TI GForge site.(Project not rated)
Dynamic Loader Reference Implementationridl_ossThis is an open source reference implementation of the dynamic loader that is covered under the TI BSD open source license restrictions. It is designed as a tesing platform that can load and run ELF dynamic applications that are built with the latest TI compilers (C6000 CGT v7.0; TMS470 CGT 4.6)(Project not rated)
Ducati System Projectducati_systemThis project focuses on developing foundation framework software for OMAP Ducati subsystem. The intent is to significantly shorten the time it may take to develop new Ducati software and to boost the comfort level with Ducati subsystem.(Project not rated)
DSP Ease of Use Development dspeasyThis project is intended to develop software and methods to simplify building and running code on the DSP core of the OMAP3 and OMAPL1 devices. Initial focus will be on using DSPLink for communicating between cores.(Project not rated)
Davinci Multimedia Application InterfacedmaiThe DaVinci Multimedia Application Interface (DMAI) is a thin utility layer on top of the operating system (Linux or DSP/BIOS) and the Codec Engine (CE) to assist in quickly writing portable applications on a DaVinci platform. DMAI is used by the DVSDK demos as of DVSDK 1.40, and is also used by the TI OMAP and Davinci Gstreamer port.(Project not rated)
CToolsLibctoolslibCTools Library(Project not rated)
CD card boot for dm3xx dm3xx_sd_bootBooting and initializing dm3xx (dm355,dm365) systems from SD card (MMC)(Project not rated)
C6474 Serial RapidIO DirectIO LibrarysriodirectiolibDIO library aims at providing a CSL-like Serial RapidIO (SRIO) "functional layer" for the directIO mode of Texas Instruments' TMS320C645x/7x DSP platform(Project not rated)
C6474 multicore nqueens demo6474_nqueensC6474 multicore demo utilizing nqueens C-code taken from Wikipedia and J. Somers running on the TI C6474 EVM. Both DSPs on the board are used and they communicate via SRIO. The package is self containing.(Project not rated)
C6474 AIF for Inter-DSP CommunicationaifinterdspDemonstration of how the AIF peripheral can be used for generic inter-DSP communication(Project not rated)
C6472 EVM On-board Demo6472evm_oobdemoC6472 On-board NAND Demo Application(s). This project page contains the original "out-of-the-box" version as well a place to add new demo ideas, modifications and branches to the original concept. (Project not rated)
C6472 EVM NAND Writer Utility6472evm_nandwrtUtility to prepare and flash on-board NAND C6472 EVM with a DSP binary image.(Project not rated)
C6472 EVM EEPROM boot utility6472evm_eepromC6472 EVM EEPROM formatting and write utility.(Project not rated)
C6472 EVM Bootloader6472evmbootloadC6472 EVM Bootloader(Project not rated)
C6472 EVM Board Support Package6472evm_bslC6472 EVM Board Support Library(Project not rated)
C6455 TCP2 and VCP2 Example codec6455tcp2Example Code for the TCP2 and VCP2 coprocessors on the C6455 or TCI6482 devices. Includes software encoders and uses hardware coprocessors for decode. Supports WCDMA turbo coding only.(Project not rated)
BitblitbitblitThis package is written to provide low level blitting/blending graphics acceleration services support. The graphics operations are accelerated using 64x+ and 674x. The package also provides an easy to use ARM side API via Codec Engine to the user. The raw BITBLIT algorithm functions have been wrapped into a XDAIS algorithm. In order for the algorithm to be used within Codec Engine the IUNIVERSAL API was implemented. A test program is included (bitblit_test) which tests each of the modes. (Project not rated)
Audio Video Examplesav_examplesThis project hosts example applications which demonstrates audio, video capture and display features of TI processors(Project not rated)
ARM Multimediaam_multimediaThis project provides example applications to evaluate ARM based multimedia on TI Sitara products(Project not rated)
ARM Microprocessor Benchmarksam_benchmarksARM Microprocessor Benchmarks: This project is intended to provide ARM performance measurement tools.(Project not rated)
ARM Crypto Supportarm_cryptoAccelerated cryptographic functions for OMAP3x/AM3x devices.(Project not rated)
Arago ProjectaragoProvides OpenEmbedded-based build framework/SDK for TI OMAP35x and DaVinci community platforms.(Project not rated)
Antenna Interface Code for C6474 IDTc6474aifAntenna Interface(AIF)Example Code for C6474 IDT Tundra(Project not rated)
Android on OMAPomapandroidThe project develops and ports Android for TI OMAP Platforms (including Zoom-1, Zoom-II)(Project not rated)
Analog Video Decoderstvp5158This project is used to support the Texas Instruments Video Decoders firmware patch and Linux driver for DM6467 and DM6446.(Project not rated)
AM system informationam_sysinfoThis project is a part of AM Matrix SDK, this will include all the scripts and projects related to the system settings application(Project not rated)