Home ยป Project Browse

Search for projects in all categories

 
 Include Trove Categories In Search

Full name
alternative text
Account name (lowercase)
alternative text
Description
alternative text
Rating
alternative text
CD card boot for dm3xx dm3xx_sd_bootBooting and initializing dm3xx (dm355,dm365) systems from SD card (MMC)(Project not rated)
C6474 Serial RapidIO DirectIO LibrarysriodirectiolibDIO library aims at providing a CSL-like Serial RapidIO (SRIO) "functional layer" for the directIO mode of Texas Instruments' TMS320C645x/7x DSP platform(Project not rated)
C6474 multicore nqueens demo6474_nqueensC6474 multicore demo utilizing nqueens C-code taken from Wikipedia and J. Somers running on the TI C6474 EVM. Both DSPs on the board are used and they communicate via SRIO. The package is self containing.(Project not rated)
C6474 AIF for Inter-DSP CommunicationaifinterdspDemonstration of how the AIF peripheral can be used for generic inter-DSP communication(Project not rated)
C6472 EVM On-board Demo6472evm_oobdemoC6472 On-board NAND Demo Application(s). This project page contains the original "out-of-the-box" version as well a place to add new demo ideas, modifications and branches to the original concept. (Project not rated)
C6472 EVM NAND Writer Utility6472evm_nandwrtUtility to prepare and flash on-board NAND C6472 EVM with a DSP binary image.(Project not rated)
C6472 EVM EEPROM boot utility6472evm_eepromC6472 EVM EEPROM formatting and write utility.(Project not rated)
C6472 EVM Bootloader6472evmbootloadC6472 EVM Bootloader(Project not rated)
C6472 EVM Board Support Package6472evm_bslC6472 EVM Board Support Library(Project not rated)
C6455 TCP2 and VCP2 Example codec6455tcp2Example Code for the TCP2 and VCP2 coprocessors on the C6455 or TCI6482 devices. Includes software encoders and uses hardware coprocessors for decode. Supports WCDMA turbo coding only.(Project not rated)
BitblitbitblitThis package is written to provide low level blitting/blending graphics acceleration services support. The graphics operations are accelerated using 64x+ and 674x. The package also provides an easy to use ARM side API via Codec Engine to the user. The raw BITBLIT algorithm functions have been wrapped into a XDAIS algorithm. In order for the algorithm to be used within Codec Engine the IUNIVERSAL API was implemented. A test program is included (bitblit_test) which tests each of the modes. (Project not rated)
Audio Video Examplesav_examplesThis project hosts example applications which demonstrates audio, video capture and display features of TI processors(Project not rated)
ARM Multimediaam_multimediaThis project provides example applications to evaluate ARM based multimedia on TI Sitara products(Project not rated)
ARM Microprocessor Benchmarksam_benchmarksARM Microprocessor Benchmarks: This project is intended to provide ARM performance measurement tools.(Project not rated)
ARM Crypto Supportarm_cryptoAccelerated cryptographic functions for OMAP3x/AM3x devices.(Project not rated)
Arago ProjectaragoProvides OpenEmbedded-based build framework/SDK for TI OMAP35x and DaVinci community platforms.(Project not rated)
Antenna Interface Code for C6474 IDTc6474aifAntenna Interface(AIF)Example Code for C6474 IDT Tundra(Project not rated)
Android on OMAPomapandroidThe project develops and ports Android for TI OMAP Platforms (including Zoom-1, Zoom-II)(Project not rated)
Analog Video Decoderstvp5158This project is used to support the Texas Instruments Video Decoders firmware patch and Linux driver for DM6467 and DM6446.(Project not rated)
AM system informationam_sysinfoThis project is a part of AM Matrix SDK, this will include all the scripts and projects related to the system settings application(Project not rated)
 

Page: < Previous 1 2 3 (70 Total Records)