Home ยป Project Browse

Search for projects in all categories

 
 Include Trove Categories In Search

Full name
alternative text
Account name (lowercase)
alternative text
Description
alternative text
Rating
alternative text
WilLink8 Releasewilink8_filesShare and hold Wilink8 release files(Project not rated)
WiLink Connectivity Drivers for OMAPwilink_driversProject develops Open source drivers for TI's WiLink (including WL1271) Solution for OMAP. (Project not rated)
Titan - Texas Instrument Test AutomatioNtitanTitan is a Test Automation Tool powered by Java and developed to run Linux Kernel test cases.(Project not rated)
TIMotorLIBtimotorlibThe aim of this project is to introduce TIMotorLIB. TIMotorLIB is an open source library in the terms of LGPL license. The proposal of this library is to achieve fast development of digital control systems, mostly focused on the control of power converters, using Texas Instruments TMS320F28XXX Digital Signal Controllers (DSC) based boards. The development of this code has been done using the eZdsp F28335 board from Spectrum Digital. The library is programmed using C as the main language, although additional contents can be developed using TMS320C28x assembler (F28XXX CPU).(Project not rated)
TI81xx A8 Host Utilitiesti81xx_a8utilsTI81xx A8 Host Utilities are a set of useful utilities which can be used by users for debug and profiling from A8 Host side on TI81xx platform. Currently its implemented and tested for TI816x but is portable to TI814x. Includes utilities for - Remote Processor Printf - DDR/L3 System Priority Set/Get - Register / Memory Rd/Wr - Ethernet + SATA use-case profiling - EDMA user space exported APIs - Syslink load and debug utilities(Project not rated)
TI OMAP4 Blaze TabletblazetabletThe project develops and ports Android for TI OMAP4 Blaze Tablet Platform.(Project not rated)
TI Embedded Speech RecognizertiesrThe TI Embedded Speech Recognizer (TIesr) is a set of fixed-point APIs implementing speech recognition. It balances resource usage, robustness to environment, and performance, and has an easy-to-use interface. This makes TIesr an excellent recognizer for developing a wide variety of voice-enabled embedded applications.(Project not rated)
Symbian Foundation on OMAPZoomomapsymbianTI ZoomII baseport for Symbian^3(Project not rated)
Support ProjectsupportSite Support Project(Project not rated)
SteelheadsteelheadThis is a project to support Google Nexus Q running AOSP Android on top of TI 3.0 kernel(Project not rated)
Sitara Flash ToolsitaraflashtoolSitara ARM Microprocessors Flash Tool for AM335x and following devices.(Project not rated)
SGX GraphicsgleslayerThis project provides necessary additional packages for Graphics software from TI. This currently includes XgxPerf - a development and performance benchmarking toolkit for Qt framework and SGXPERF for SGX530. A GLES renderer for the OGRE3D Gaming Engine is already part of OGRE mainline. (Project not rated)
qt-demosqt-emb-demosqt based demos for arm embedded processor(Project not rated)
PRU Softwarepru_swSoftware for TI's Programmable Real time Unit (PRU), including Linux driver & samples(Project not rated)
Pin Setup for AM18xxpinsetup_am18xxPin setup utility for AM18xx devices(Project not rated)
Pin Mux Utility for Sitara ARM MPUpinmuxutilitySoftware tool for evaluation of pin muxing options for Sitara ARM MPU and related devices.(Project not rated)
panda-binariespanda_binariespandabord binary files(Project not rated)
OpenMax for OmapopenmaxThe project contains TI's OMX components written on top of accelerated DSP codecs. (Project not rated)
OpenLinkopenlinkTI's wireless solution for community(Project not rated)
omapreg_debugomapreg_debugThis module provides read/write access to the complete system space using the DebugFS interface. This is similar to devmem2 userspace tool. But certain registers in OMAP architecture can be accessed only in supervisor mode. This tool provides this using the DebugFS interface. For example, the pinmux registers in DM816x and DM814x platform cannot be written from userspace. This module will be helpfull in this case. This is just a debug module which could build separately and used. The same module should also work on all 32-bit CPU architectures (not only ARM/OMAP).(Project not rated)
OMAPpediaomappediaFiles and Docs for Omappedia.org(Project not rated)
OMAP ZoomomapzoomSupport collaboration around the OmapZoom MDP.(Project not rated)
OMAP SYSLINK / BIOS IPCsl_bios_ipcBIOS IPC in Syslink includes the inter-process communication components running on the subsystems, i.e. DSP or Cortex-M3.(Project not rated)
OMAP Support ToolsomaptoolsOMAP Support Tools(Project not rated)
OMAP SGX Graphics Drivers for AndroidomapgraphicsThis project maintains the Graphics SDK for the OMAP3/4 platforms running the Android OS(Project not rated)
 

Page: 1 2 3 Next > (70 Total Records)