Home ยป Project Browse

Search for projects in all categories

 
 Include Trove Categories In Search

Full name
alternative text
Account name (lowercase)
alternative text
Description
alternative text
Rating
alternative text
Matrix TUI Launcher Applicationmatrix_tuiThe Matrix TUI (Text User Interface) is the complement UI to the Matrix GUI project. Using ncurses, it is designed to provide a text user interface on the console that creates a hierarchy and ease of use for the example applications and demos that exists in the TI ARM Cortex-A8 SDKs. It's functionality and available applications & demos mirrors that of Matrix GUI. The TUI uses a .xml file which is parsed by libxml to create the main menu and supported submenus. Like the Matrix GUI, additional applications and demos may be added by simply modifying the existing .xml file. (Project not rated)
Matrix GUI Launcher Applicationmatrix_guiThe Matrix GUI is a launcher application being developed for the TI ARM based SoCs. The GUI is a simple .html page that is developed using Qt/webkit. The 3x4 or 2x4 matrix of icons calls existing example applications and demos and makes them accessible to the user. Additional applications or demos may be easily added by simply modifying the existing .html file. The GUI is touchscreen, mouse and keyboard enabled and enhancements can be made by the users using the Qt SDK. Matrix is intended to address the ease of use and quick OOB experience. It is also meant to serve as the baseline for our SDKs that will allow users to extend existing applications or create their own. (Project not rated)
Matrix Application Launcher v2matrix-gui-v2The Matrix GUI is a launcher application being developed for the TI ARM based SoCs. The 3x4 or 2x4 matrix of icons calls existing example applications and demos and makes them accessible to the user. Additional applications or demos may be easily added by simply adding a new desktop file into the target file system and refreshing Matrix. Matrix works either by touchscreen or mouse and keyboard on the target or remotely through an external browser. Matrix is intended to address the ease of use and quick OOB experience. It is also meant to serve as the baseline for our SDKs that will allow users to extend existing applications or create their own.(Project not rated)
Low Level Driver Exampleslld_examplesThis project contains examples for programming the EDMA3 with the LLD (low-level driver) library.(Project not rated)
IPCipcIPC - discussion for projects hosted at http://git.ti.com/ipc/ipcdev(Project not rated)
 

Page: < Previous 1 2 3 4 5 6 7 8 9 10 11 12 13 14 Next > (70 Total Records)